Hello All,
I am new in this forum, please let me know if I need to do certain things, or have some mistakes in asking question.
Currently I am using https://www.mikroe.com/rs485-isolator-2-click which is based on ADM2867E and has schematics here https://download.mikroe.com/documents/add-on-boards/click/rs485_lsolator_2_click/rs485-isolator-2-click-schematic-v101.pdf , and I am currently facing a problem.
My purpose is to have a communication between MCU with 3.3V and RS485 devices on different voltage system and ground (Isolated system)
I have connected RE/DE together as I am using Half Duplex for this communication
I did not receive any reaction from the RS485 device, so I was troubleshooting the MikroE board when I found out that there is no output on A B side

If you see the picture above the color is listed as below:
Yellow - B
Purple - A
RE/DE - Blue
TX - Green
From the picture above, the TX is not translated at all to the other side of RS485 A B.
After I scope it several times, I also found out that some of the signal actually passed through
Ignore the blue and green as I forgot to connect it this time
About the Board itself, I am connected the YZ and the AB as it is half-duplex and connected J7 J8 and J9 in the isolator schematics (link on top)
Please help me on my problem.
Thank you!