Post Go back to editing

ADN4655 LVDS Voltage Levels

Thread Summary

The user is using the ADN4655 to isolate a SerDes interface between two FPGAs with different common mode voltages (1.2V and 0.6V). The ADN4655 can reliably transfer signals as long as the input differential voltage (VID) is more than +/-100mV. The output common mode voltage of the ADN4655 is 1.17V, and AC coupling is recommended if FPGA2 applies a different common mode voltage at its differential input termination.
AI Generated Content
Category: Software
Product Number: ADN4655
Software Version: NA

I am using the ADN4655 to isolate SerDes interface between two FPGAs. One FPGA#1 has Vcm =1.2V and Vd = 350mV while the other FPGA#2 has Vcm = 0.6V and Vd = 550mV.

I am understanding that the ADN4655, since isolated, translation between the two LVDS interface should be feasible.

For the input, as long as the (Vid) swing is more than +/-100mV threshold regardless of the common mode voltage, the receiver will work and understand low and high logic. Correct?

For the output, the Vod is +/-(250mV-450mV), correct? Now assuming there is no AC coupling, what will the common mode voltage be for the output signals? Is it going to be based on the common mode of the FPGA so in FPGA#1 1.2V and FPGA#2 0.6V or is it a constant voltage of 1.17V and AC coupling should be used to level to FPGA#2 voltage?

Edit Notes

clarified
[edited by: SS636 at 11:05 AM (GMT -4) on 15 Jun 2022]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.