Post Go back to editing

ADM3052 operation in non-isolated use case

Thread Summary

The user inquired about using the ADM3052 in a non-isolated application instead of the ADM3051 due to availability issues. The final answer confirmed that it is acceptable to connect GND1 and V- on the ADM3052 for non-isolated operation. No additional critical clarifications were provided in the accompanying answers.
AI Generated Content
Category: Hardware
Product Number: ADM3052

We have one design using the ADM3052 in an isolated design and due to availability issues along with a very limited production run would like to use it in a an non-isolated application that would normally call for use of the ADM3051.  Can we use the ADM3052 in a non-isolated power application, and is there a sample circuit topology for doing so?  Or is there a technical reason why GND1 should not be tied to V-?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.