Hi,
I am using ADP1031 to generate 15V, -15V and 5.15V from a 24V input voltage.
The voltages are generated correctly but when I check the FFT Spectrum, I notice unwanted peaks at certain frequencies.
Here are screenshots from my measurements:
24V input without connecting to the PCB yet:
24V input after connecting it to the PCB:
I have another switching regulator (L7983PU33R) on my design.
So, I tested another PCB after I removed the L7983PU33R from the board and measured 24V input again:
Then I took another PCB and removed ADP1031 and kept L7983PU33R on the board. I measured the 24V input again:
On another question in the forum, I saw that you suggested to add resistors to the output of ADP1031 so that it does not go into the power saving mode.
So, I added 1k resistors between 15V and GND, -15V and GND and 5.15V and GND.
Then I measured the 24V input again:
These measurements show the 24V input of the ADP1031 but the outputs also look similar, for example:
15V output:
-15V output:
5.15V output:
Do you have any suggestions on how I can remove these unwanted noise?
Should I add low pass filters to all three outputs of ADP1031?
Thank you very much for your help and best regards.
Changed category from software to hardware
[edited by: bahadirdonmez at 8:52 AM (GMT -4) on 30 May 2022]