ADuM5411
Production
The ADuM5410/ADuM5411/ADuM5412 are quad-channel digital isolators with isoPower®, integrated, isolated dc-to-dc
converters. Based on the Analog Devices...
Datasheet
ADuM5411 on Analog.com
I use the ADUM5411 for isolate 3.3V and 5V logic.
so I designed circuit as following :
I konw that the VDD1 is a voltage Input pin, but VDD1 is measured 4V.
3V3_MAIN is my board's main power, but it's voltage go up to 4V cause VDD1.
I know that VDD! is indpendent of VDDP as datasheet :

I don't know what's the problem??
I want to know if tthere is a any problem on my curcuit?