Post Go back to editing

About ΘJa of 2 kinds of packages of ADuM6000

Category: Datasheet/Specs
Product Number: ADuM6000

Hi,

I am considering the ADuM6000.

I have a question about ΘJa.

This IC has two types of packages, 16-SOIC_IC and 16-SOIC_W.

The two packages are different, but only one ΘJa listed in Table 5 is 45 °C/W.

Are both packages ΘJa = 45 °C/W ?

Best regards,

Yuya

Parents
  • The thermal impedance of the two packages will be nearly the same. Keep in mind that the thermal impedance is dependent on many factors including PCB layout and ambient temperature, the thermal impedance listed is based on a JEDEC 2s2p thermal simulation under typical operating conditions (5V in, 5V out at rated load current).

Reply
  • The thermal impedance of the two packages will be nearly the same. Keep in mind that the thermal impedance is dependent on many factors including PCB layout and ambient temperature, the thermal impedance listed is based on a JEDEC 2s2p thermal simulation under typical operating conditions (5V in, 5V out at rated load current).

Children