Post Go back to editing

ADuM160N/161N About UL standard protection (single / double)

Hi,

I have a question about ADuM160N / 161N.

The D / S has the following explanation.
"Double Protection, 3000 V rms Isolation Voltage"

https://www.analog.com/media/en/technical-documentation/data-sheets/ADuM160N-161N-162N-163N.pdf#page=13

I also checked "File E214100" which is also described in D / S.
I found the document on UL's site,
Only the explanation about "Single Protection" was written here.

iq.ulprospector.com/.../profile

Which is correct?
Please let me know because it is necessary to support "Double Protection" in this development.

Best Regards,

Naohisa