Post Go back to editing

LT3960 :: Multi slave connection

Hello,

I would like to use a LT3960 as I2C to CAN transciever, because of a long distance between mCU (master) and sensor (slave) devices.
I would like to have isolated mCU ground from sensors device ground, so I'm planning just to connect CANSDAH, CANSDAL, CANSCLH and CANSCLL lines in between.
Some slave devices will be connected via connector, so communication lines (CANSDAH, CANSDAL, CANSCLH and CANSCLL) would go through the connector. Is it recommended to use a magnetics/transformer in such example (is it better to place magnetics near the slave or master device)?
Is hot-pluging covered/supported or is needed to use for. ex. ADuM1251 in a series with a slave LT3960 which is connected to the master LT3960 via connector?
Basic schematic:

Many thanks,
Kind regards,
Dejan.

Parents Reply
  • Hi Dejan,

    Please allow me to correct my previous statement. 

    It is not necessary to connect the GND of the master and slave LT3960 together as long as the common-mode range of I2CAN busses doesn’t exceed the limit for the provided supply voltage (+/-25V for 3.3V VCC, +/-36V for 5V VCC).

    Regards, 

    Peter Pham

Children
No Data