LT3960
Recommended for New Designs
The LT3960 is a robust high speed transceiver that extends a single-master I2C bus through harsh or noisy environments at up to 400kbps using the CAN-physical...
Datasheet
LT3960 on Analog.com
ADUM1251
Production
The ADuM1250/ADuM1251Â are hot swappable digital isolators with non-latching, bidirectional communication channels that are compatible with I2C interfaces...
Datasheet
ADUM1251 on Analog.com
Hello,
I would like to use a LT3960 as I2C to CAN transciever, because of a long distance between mCU (master) and sensor (slave) devices.
I would like to have isolated mCU ground from sensors device ground, so I'm planning just to connect CANSDAH, CANSDAL, CANSCLH and CANSCLL lines in between.
Some slave devices will be connected via connector, so communication lines (CANSDAH, CANSDAL, CANSCLH and CANSCLL) would go through the connector. Is it recommended to use a magnetics/transformer in such example (is it better to place magnetics near the slave or master device)?
Is hot-pluging covered/supported or is needed to use for. ex. ADuM1251 in a series with a slave LT3960 which is connected to the master LT3960 via connector?
Basic schematic:
Many thanks,
Kind regards,
Dejan.
Hi Dejan,
The LT3960 can support hot plugging as long as there are 120ohm termination resistors next to the LT3960 master and LT3960 slave 1 as shown below. You don't need termination resistors or I2C isolation for LT3960 slave 2 and 3.

Regards,
Peter Pham
Hello Peter,
thanks for your reply.
So, in connecton you proposed, there is no need to connect grounds of separated together?
According to the picture on the first page of LT3960's datasheet, difference between ground voltages should be less than 25 V (at VCC=3.3 V) or did I miss something?
Many thanks,
Kind regards,
Dejan.
LT9360 ground pins have to be connected like in the datasheet.
Regards,
Peter Pham
Hello,
but I really need to have isolated power supply grounds (like shown in schematic in the first post). Should I use I2C isolator like ADuM1251 or equivalent between each LT3960 and sl ave device if a power supply grounds of all LT3960 must be connected together?
Many thanks,
Kind regards,
Dejan.
Hi Dejan,
Please allow me to correct my previous statement.
It is not necessary to connect the GND of the master and slave LT3960 together as long as the common-mode range of I2CAN busses doesn’t exceed the limit for the provided supply voltage (+/-25V for 3.3V VCC, +/-36V for 5V VCC).
Regards,
Peter Pham