Post Go back to editing

LTC4310 communication issues

Thread Summary

The user is experiencing unreliable communication with two LTC4310-2 devices in a 100kHz I2C network, despite the devices being rated for 400kHz. The final answer confirms that the LTC4310-2 can operate at lower speeds, suggesting the issue may lie elsewhere in the system configuration.
AI Generated Content

I'm using two LTC4310's in an identical configuration to that shown in the datasheet example but I'm not getting reliable comms across the system( the device fails to acknowledge at all). As voltage limits look correct on the digital sending and receiving side I am left thinking that the system I am using is communicating at 100kHz not 400 kHz ( which is the version of the part I am using) . My assumption was that the higher speed part could be used on a lower speed network. Is this assumption correct or is this the basis of the error? Does the 400kHz part work on a 100kHz network.

Thanks a lot

Richard