Post Go back to editing

ADUM3153 SPI confusion

Hello everyone,

I want to establish a SPI communication between my Raspberry Pi Zero (Master) and the Energy meter ADE 7753 (Slave). For that i need an SPI isolator, in my case it is a ADUM3153 with 3.3V on primary side and 5V on the secondary side(isolated). When I measure the SPI signals on the primary side, without the ADE 7753 connected (just RPi and SPI Isolator), I am getting the following:

I am wondering how is it possible that I am seeing the delayed MOSI signal on the MISO line? Is there any explanation for that?
For me it looks like as if the MOSI and MISO are coupling internally. I also checked the connections for shorts.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.