Post Go back to editing

Using LTC2873 with VEE = 0V

Is it possible to run LTC2873 with external Vdd = 5V and Vee = 0 V supplies? The target is to use RS485 normally but to get RS232 output voltage levels to 5 V and 0 V. Then the RS232 mode would provide a general 0V/5V GPIO not fulfilling the RS232 specs.