Post Go back to editing

What is the permitted current into any pin of digital isolator ADuM242E1BRIZ that will not damage the isolation characteristics?

I have an application where I need to protect the isolation of a digital isolator in the event a fault in either of the two circuits that it couples.

To achieve this goal

  1. The left hand side circuit will limit the voltage supply of the left hand side in the event a fault in the left hand side circuit.
  2. The right hand side circuit will limit the voltage supply of the right hand side in the event a fault in the right hand side circuit.
  3. Each input and output has a protective impedance that will limit the current into or out of a pin in the event a fault and also during normal operation.

Note that in the event of a fault it is acceptable for the digital isolator to stop working but the isolation characteristics must be preserved however.

The data sheet for the ADuM242E1BRIZ  in the section "DIN V VDE V 0884-10 (VDE V 0884-10) INSULATION CHARACTERISTICS" states that 2.78W can be dissipated without damaging the insulation.  However it does not state how much current can flow into or out of pin without damaging the insulation.

On the other hand, if I look at the data sheet for MAX22444–MAX22446, in the section Safety Limits, it states that "Safety Current on any pin = 300mA".  This is the information I need!

It would also be helpful if you described the structure of the input and output pins (I assume conventional CMOS) and a gave a figure for the current that the clamp diodes (I assume that there are clamp diodes) can conduct under normal operation.