Post Go back to editing

ADM3067E / ADM3068E

Thread Summary

The user inquired about the minimum cable length for achieving a 50 Mbps data rate with the ADM3067E or ADM3068E transceivers. The final answer confirms that 50 Mbps over 10 meters is within the performance bounds, with these devices capable of maintaining a total jitter of less than 30% of the 20ns unit interval over up to 50 meters using a PRBS-7 pattern. The article at [URL] provides additional relevant details, though it focuses on the ADM3065E.
AI Generated Content

Dear experts,

My project needs a transceiver with 50 Mbs data rate so I thought about ADM3067E or ADM3068E.

The question is:

what is the minimum length of a cable to have that data rate? Is it possible to use a 5m  or 10m cable?

I've read datasheet but there are not answers about this argument.

Best regards,

  • In general, the maximum cable length at these data rates is limited by attenuation and inter symbol interference effects introduced by the cable. For a given transceiver, the max cable length for a given data rate is dependent on the jitter budget at the receiving node, as well as other factors such as the cable attenuation and encoding scheme used.

    For the ADM3067E/68E, 50 Mbps over a 10 meter cable is well within the performance bounds , so there should be no issue. These devices can communicate at 50 Mbps over up to 50 meters while maintaining a total jitter of less than 30% of the 20ns unit interval, when tested with a PRBS-7 pattern.  

    Some more details are covered in this technical article. The article discusses results with the ADM3065E but the results are also relevant to the ADM3067E and ADM3068E, which use the same silicon. 

    https://www.analog.com/en/technical-articles/going-faster-further-with-fieldbus.html

    Kind Regards,

    Neil 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.