Is the inrush current range on the ADM2487E documented anywhere? We have some product that are not working properly. On powerup, the unit draws too much current that our 3.3V LDO goes into a foldback mode and just draws a lot of current. I tested two parts on a bench supply, one powered up on 3.3V w/ a 50mA current limit setting, and the other (problem part) required 3.3V with a 750mA current limit setting. We are using the coilcraft DA2303-AL transformer. Any thoughts?
Edit Notes
corrected p/n[edited by: sel82 at 4:29 PM (GMT -5) on 16 Jan 2022]