Hello,
I am using the ADN4654 to isolate MIPI CSI-2 (High speed only) and believe the ADN4654 inputs are compatible but the ADN4654 outputs require AC caps to remove the DC offset for the MIPI receiver.
My circuit is:
DS90UB960-Q1 --> ADN4654 (100 ohm resistor across inputs) --> FPGA CSI-2 receiver (.1uF AC cap for each input).
Below are the datasheet screenshots for all 3 chips.
Are 100 ohm differential resistors across the ADN4654 inputs and AC caps on the ADN4654 outputs all that is needed?
Thanks,
Tim
DS90UB960:
ADN4654:
FPGA: