Post Go back to editing

Input voltage at bus terminal of these RS485 transceivers LTC2862H

Hi. 

What is the input voltage at bus terminal of LTC2862H?

We have our own special application on RS485 transceiver like below,


RS485 Master: connect B to GND and connect A to 12-16V.

RS485 Slave: one(can be A or B) to GND minus one diode and one(can be A or B) to 12-16V (possible 24V) minus one diode.

Will the LTC2862H be able to handle LTC2862H with the application above?