Post Go back to editing

Looking for alternate Part: ADN4650BRWZ-RL7

Dear Sir/Madam

Can you suggest the alternate part number for ADN4650BRWZ-RL7,



Can you suggest the alternate part number for ADN4650BRWZ-RL7,
[edited by: mukesh at 12:38 PM (GMT -4) on 20 Oct 2021]
Parents
  • Hi Mukesh,

    An alternative for ADN4650 is ADN4654, same pinout and functionality but rated for up to 1.1Gbps data rate rather than 600 Mbps maximum. Part numbers are ADN4654BRWZ and ADN4654BRWZ-RL7.

    If you are working on a new design/PCB, another option is the recently released ADN4624, similar wide SOIC package option but with four channels at up to 2.5 Gbps. Part numbers ADN4624BRNZ and ADN4624BRNZ-RL. Or if the isolation needs are just basic/functional at lower voltage, 6x6 mm LFCSP option ADN4624BCPZ and ADN4624BCPZ-RL.

    Best regards,

    Conal

Reply
  • Hi Mukesh,

    An alternative for ADN4650 is ADN4654, same pinout and functionality but rated for up to 1.1Gbps data rate rather than 600 Mbps maximum. Part numbers are ADN4654BRWZ and ADN4654BRWZ-RL7.

    If you are working on a new design/PCB, another option is the recently released ADN4624, similar wide SOIC package option but with four channels at up to 2.5 Gbps. Part numbers ADN4624BRNZ and ADN4624BRNZ-RL. Or if the isolation needs are just basic/functional at lower voltage, 6x6 mm LFCSP option ADN4624BCPZ and ADN4624BCPZ-RL.

    Best regards,

    Conal

Children
No Data