Post Go back to editing

ADM2867E RS 422 Transceiver

Thread Summary

The user asks about the necessity of connecting the isolated ground to the chassis through an RC filter when interfacing RS-422 channels between two systems. The final answer suggests that the user should share the required diagrams via email for a detailed review, as the file attachment feature is not working. The accompanying answer confirms that the files have been sent for review.
AI Generated Content

scenario 1

I am interfacing RS-422(Isolated) channels of two systems with each other and  each system has RS-422 which have five wires i.e Tx-, Tx+,Rx-,Rx+ and Ground as show in attached diagram (File name : Both_System_ADM2867)

Q1:Did we need to connect ground (isolated) to chassis through RC filter in each system (File name: Both_System_ADM2867 with RC filters) ? is it necessary? what are the advantages and disadvantages of it? or it's work okay as it is shown in diagram( File name : Both_System_ADM2867)Kindly give reason of it .

scenario 2

I am interfacing RS-422(Isolated) channels of two systems with each other 

1) one system has RS-422 which have five wires i.e Tx-, Tx+,Rx-,Rx+ and Ground

2) Second system has RS-422 which have ffour wires i.e Tx-, Tx+,Rx-,Rx+ 

as show in attached diagram (File name : Rs 422 five wires and 4 wires)

Q2: Did we need to connect ground  to chassis through RC filter in system which has five wires  ? or with out RC filter its work okay ? Kindly give reason of it .

Parents Reply Children
No Data