Post Go back to editing

ADM3056E CAN_H and CAN_L waveform

Thread Summary

The user encountered unusual waveforms on CAN HIGH and CAN LOW while using the ADM3056EBRIZ, with the issue being dependent on Rslope. The final answer suggested that the problem was due to differences in turn-off characteristics and parasitics during the dominant to recessive transition. The user found that split termination resolved the issue, improving the waveforms significantly.
AI Generated Content

Hi!

I encountered some strange waveforms while evaluating the ADM3056EBRIZ: While the differential signal looks good (purple) and communication works, CAN HIGH and CAN LOW (green/yellow) seem very odd to me.



This over/undershoot seems to be somewhat dependend on Rslope.

Rslope = 55k


Rslope = 80.9k:


There may be a point where this is balanced around 60..75k , but this is already out of spec according to Fig. 11. of the datasheet.

Any helpful idea on whats causing this?

Edit Notes

added: "Fig. 11 of the datasheet"
[edited by: patteb at 1:29 PM (GMT -4) on 30 Aug 2021]
  • Hi Pat, 

    Looks common-mode. What's the applications termination circuit look like? Split termination with a filter cap? Are the network cables very long or transceivers being supplied from independent sources? 

    Regards,
    Jason

  • Hi Jason,

    yeah, definitely common mode. The bus is on both ends terminated with 120R across CANH and CANL. Cables are unshielded but quite short : the longest one is just about 1m (about 3ft).

    The bus sides of the trancievers share a common supply of 5V. Power and ground are also distributed on the same cable as the signals but are clean. Logic sides are of course supplied by individual supplies, therefore the isolator.

    [EDIT]

    Well, sometimes it's the simple(-ish) things. I just tried split termination and now everything looks fine.

    Do you have any input on what I was seeing? It did not register as high-frequency noise or anything reflection-related to me, so I still don't see why the low-pass of the split termination is so obviously beneficial.

    Thank you for your time and kind regards,

    Patrick

  • Hi Patrick, 

    Its not high frequency noise or reflections. During the dominant to recessive transition there are two different devices turning off quickly. Any difference in the turn off characteristics will translate into common-mode voltage. There may also be some difference between CANH and CANL parasitics created by the bus (layout, protection components, construction…). Those may contribute to common-mode as well. 

    Regards,

    Jason