Post Go back to editing

LTC4331, remote I2C interface doesn't respond

Hi,

I'm experimenting with the LTC4331 demo board, with my own uproc board. My setup is:

uproc <===> local LTC4331 <===> cable <===> remote LTC4331 <===> EEPROM

program is simple: continuously reading from (remote) EEPROM, filled with know data. So after each read do a compare, etc.

Initially I had spurious issues of stuck SCL, but found this article: Unexpected behavior of LTC4331 - Q&A - Interface and Isolation - EngineerZone (analog.com)
After delaying each read with at least 35ms, as suggested in the article, all went fine.

Now next step I want to experiment with the control interface of the device. I can read the local I2C device (address 0x3E), but I get NAK's from the remote device. I tried every jumper setting for A1/A2, even made a quick scan routine to find all I2C devices. But all what is reported is 0x3E and 0x50 (for the remote EEPROM).

Q1: Is the remote I2C device suppose to respond on I2C register access?
Q2: Is the Packet Error Correction also applicable for the data transfer from my remote EEPROM to the local LTC4331? Or is PEC only used for transfers from uproc to the LTC4331 control interface?
Q3: related to Q2, if any bit error occurs in the transfer from reading my remote EEPROM to the local LTC4331, will that be detected as a 'fault'?

regards,
_Wim_

Parents Reply Children
No Data