Post Go back to editing

ADUM1411 with unpowered VDD1

Hello,

I'm using 12pcs. ADuM1411 in oder to drive isolated ADCs with a single SPI. In my design I connected MISO to V_OD of all ADuMs.

The Idea was to use a transistor to power up VDD1 only when needed (i.e. when CS goes low).

Looking at the truth table in the datasheet, V_OD should go High-Z when VDD1 is unpowered and the output pins V_OA, V_OB and V_OC should go high (assuming CTRL1 is unconnected).

But this is not the case. Even with VDD1 completely disconnected the ADuM is still passing signals from V_IA to V_OA and VDD1 is **sourcing** 2.4V!! Only when I tie VDD1 to GND1 I can see the specified behavior (but then I have 50mA(!) running from VDD1 to GND1).
Is there anything I'm missing here?

Thanks in advance!

Detlef

Parents
  • Hi Detlef,

    VOD should go High-Z when Vdd2 is powered and Vdd1 is unpowered. That means VOA , VOB and VOC will have their input side (Vdd1) unpowered, and output side (vdd2) powered so these outputs will be in the default state, determined by the CTRL2 (Not CTRL 1). If CTRL2 is unconnected or high then VOA VOB and VOC will go high. CTRL1 controls VOD not VOA VOB AND VOC.

    Regards,

    Naveen

  • Thanks for your quick response.

    But VOD doesn't go High-Z when Vdd2 is powered and Vdd1 is unpowered as long as VIA, VIB or VIC are still receiving signals. I'm using VIA and VIB for CLK and MOSI in parallel to all ADUMs

    Pin1 is not connected. If pulled to GND VOD goes high-Z, but I see 50mA running from pin1 to gnd.

Reply
  • Thanks for your quick response.

    But VOD doesn't go High-Z when Vdd2 is powered and Vdd1 is unpowered as long as VIA, VIB or VIC are still receiving signals. I'm using VIA and VIB for CLK and MOSI in parallel to all ADUMs

    Pin1 is not connected. If pulled to GND VOD goes high-Z, but I see 50mA running from pin1 to gnd.

Children
No Data