Using ADM2682E in long distance

when i use ADM2682E between two nodes of which the distance is more than 100m, do i need to connect the two GND2 of ADM2682E to provide reference? Or just connect the bus pins of two ADM2682E chips with termination resister is ok ?