ADM3054 Common Mode Voltage

Hi,

I'm looking at the ADM3054 isolated CAN transceiver and I did not find the common mode voltage specification for the bus side. To clarify the spec I am looking for: the max voltage of CANH or CANL measured in reference to GND2, that still allows the device to work normally. Please do not confuse this with the Absolute Maximum Rating spec (which I did find). I do not ask above what voltage the chip may die - rather, I ask below what voltage the chip is guaranteed to operate normally. This is typically quite lower than the Absolute Maximum Rating, and I did not find it in the datasheet.

best regards,

Guy.