What is value of maximum Tc(Case temperature) and Junction to Board Resistance(R_θJB)?
Edit Notes
Maximum value of Tc needed[edited by: RamaManikandan at 11:13 AM (GMT -4) on 26 May 2021]
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
What is value of maximum Tc(Case temperature) and Junction to Board Resistance(R_θJB)?
Hi RamaManikandan,
TJMAX or the Max Case temperature = 150°C
The junction-to-case thermal resistance of the LTC2870IFE is 5-10C/W. I believe it's been answered before. LTC2870IFE junction-to-case resistance - Q&A - Interface and Isolation - EngineerZone (analog.com) I don't think we have the R_θJB metric for this 38 -lead TSSOP package. I will confirm this with the assembly/packaging engineer and get back to you.
Regards,
Naveen
Junction to board thermal resistance is approx 34-39°C/W.
Regards,
Naveen
Hi Naveen Afzal,
I was confused because you have mentioned R_θJB as value for 38-Lead Plastic TSSOP in your first comment.
Please acknowledge once that you have mentioned Tc(max) and R_θJB you have mentioned is for LTC2870IFE#PBF 28-Lead Plastic TSSOP.
And Kindly also attach the value of Power dissipation value of LTC2870IFE#PBF.
Hi,
Junction to board thermal resistance for the 28-Lead TSSOP is 34-39°C/W and TJ max is 150°C. I rechecked. The power dissipation will depend on the operation conditions too. It is approx 632 mW (worst case).
Regards,
Naveen
Thanks for the quick reply Naveen Afzal
Whether PDML file is available for this component. If yes please attach the file.
Hi Naveen Afzal
Please explain at what condition this high power dissipation of 632 mW will occur and also kindly provide the Power consumption for that same condition.
Please explain at what condition this high power dissipation of 632 mW will occur and also kindly provide the Power consumption for that same condition.
Hi RamaManikandan,
We don't have that file available for this part.
Regards,
Naveen
Hi RamaManikandan,
Max power consumption is 632 mW (worst case at -40degC and max rate 20mbps). That figure can be estimated from the datasheet. 
Max power dissipation is around 253 mW as there will be a power dissipated across the termination load. You can see this from the datasheet too. (3.7V & 54 ohm load) when it is in RS485 mode (worst case) . A logic high on the 485/232 pin enables the RS485 mode.

Regards,
Naveen
Can you please provide the Maximum Power Dissipation value for LTC2870IFE at 3.3V supply.
In the Previous comments it seems like you have calculated with help of Load resistance seen by the driver. But how can we consider only this load resistance of driver while calculating the entire Power dissipation of the device? Is this methodology of calculating maximum power dissipation of entire IC is correct? Kindly explain