If two enables EN1 & EN2 are high at the same time which INPUT will be considered for output?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LTC4314
Production
The LTC4314 is a hot-swappable 4-channel 2-wire bus multiplexer that allows one upstream bus to connect to any combination of downstream busses or channels...
Datasheet
LTC4314 on Analog.com
If two enables EN1 & EN2 are high at the same time which INPUT will be considered for output?
Hi Diode,
Both. Each of the LTC4314 multiplexer's ENABLEx pins is going to connect(or disconnect) the corresponding SCLOUTx/SDAOUTx bus segment. So if both ENABLE1 and ENABLE2 are driven high, the LTC4314 device is going to connect both SCLOUT1/SDAOUT1 and SCLOUT2/SDAOUT2 to SCLIN/SDAIN
Regards,
Jason
Hi Jason,
Could you please suggest a part? Like Priority based I2C multiplexer. In my case EN1 is high and if EN2 is pulled high there be no operation until EN1 is released.
Thanks
Dharma
Hi Dharma,
No such part to my knowledge. The LTC4306 would be another type of I2C multiplexor... the '4306 sets the connections by commands from the IN bus segment rather than using enable pins.
Is this a multi-master system, or do you have multiple slaves with non-unique addresses? Could you describe what you are trying to accomplish with this application?
Thanks,
Jason
Thank you Jason.
Thank you Jason.