Hi,
I am planning to use ADUM6020-5BRIZ for Isolated CAN interface implementation. I am confused about the Output Supply Current of the ADUM6020-5BRIZ.
In the datasheet it is stated as given below.
| Parameter | Symbol | Min | Test Conditions/Comments |
| Output Supply Current | IISO (MAX) | 50mA | 4.75 V < VISO < 5.25 V |
| 100mA | 4.5 V < VISO < 5.25 V |
I will use an Isolated CAN Transceiver which requires 4.75V(min )- 5.25V(max) supply voltage and at least 73mA supply current.
For ADUM6020-5BRIZ, which "Output Supply Current" value (50mA or 100mA?), I should take into account. Since 4.75V(min )- 5.25V(max) value is also in the range of 4.5 V < VISO < 5.25 V, is 100mA value valid for my case?
Thanks in advance
Best regards.