Post Go back to editing

LTM2810-S Impedance State

Hi,

Does the pin 'ON (A4)' at Logic LOW turn off the power on the isolated side? what is the impedance state of O1, O2P and O3 on the isolated side when the ON is set to LOW? thanks. 

ST1, ST2 (A6, C6): Bridge Driver Outputs, Referenced
to PVCC and GND. Each output runs at 50% duty cycle,
ST1 is 180 degrees out of phase with ST2. Operating
frequency is 2MHz. Bridge driver is enabled when PVCC
is between 3V to 5.5V and ON is high.

Parents Reply Children
No Data