CAN bus transceiver - SAE -J1939 CAN BUS

Hi ADI pals, 

Which ADI part number is for CAN bus transceiver and meet SAE-J1939 spec for automotive application?

Can LT3960 (I2C to CAN) meet SAE J1939 spec ? 

BRs,

Parents
  • +1
    •  Analog Employees 
    on Feb 16, 2021 3:11 AM 12 days ago

    Hi gen, 

    J1939 is based on the ISO11898-2 physical layer. For automotive applications, there may also be an AECQ100 requirement. The ADM3054W is the only automotive qualified CAN transceiver in the ADI portfolio.

    The LT3960 is designed to service the I2C bus. It does not comply with the protocol requirements of J1939 or communicate with any standard CAN frame.  

    Regards,

    Jason

Reply
  • +1
    •  Analog Employees 
    on Feb 16, 2021 3:11 AM 12 days ago

    Hi gen, 

    J1939 is based on the ISO11898-2 physical layer. For automotive applications, there may also be an AECQ100 requirement. The ADM3054W is the only automotive qualified CAN transceiver in the ADI portfolio.

    The LT3960 is designed to service the I2C bus. It does not comply with the protocol requirements of J1939 or communicate with any standard CAN frame.  

    Regards,

    Jason

Children
No Data