Hi ADIexpert
I use ADUM3160 to isolate USB data from my CPU to external USB device (in my test, it's a keyboard)
please see my test circuit and configuration below
-
---------------------
upstream
VBUS1: 5V
VDD1/PDEN/SPU: 3.3V
---------------------
douwnstream:
Vbus2/VDD2/SPD/PIN: 3.3V
----------------------------
Also, I added a 10k pull up resisitor to Vbus2 at DD+ ( the idea is from the issues on EZ zone )
but the communication is still failed
This is my test waveforms
1. the waveform when keyboard is attached to the USB port (power on)
2. In win10, I rescan the USB device to try to make communication between host and device
but it looked like the UD- can't pull low under VIL of ADUM3160
I tried to remove the isolator, the signal UD- can pull low to around 0V and the keyboard device was successfully detected in Win10
any idea about the issue is appreciated
thank you
Ken