What is Max Input Logic Threshold Low RE ADM4852? What is Min Input Logic Threshold High RE ADM4852?
What is Max Input Logic Threshold Low DE ADM4852? What is Min Input Logic Threshold High DE ADM4852?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
ADM4852
Production
The ADM4850 / ADM4851 / ADM4852 / ADM4853 / ADM4854 /
ADM4855 / ADM4856 / ADM4857 are differential line transceivers
suitable for high speed, half-duplex...
Datasheet
ADM4852 on Analog.com
What is Max Input Logic Threshold Low RE ADM4852? What is Min Input Logic Threshold High RE ADM4852?
What is Max Input Logic Threshold Low DE ADM4852? What is Min Input Logic Threshold High DE ADM4852?
Hi Aleksei710,
The thresholds for both the DE and /RE pins are as follows:
– Max low threshold: 0.8V
– Min high threshold: 2V
Best Regards,
Shane
Hi Aleksei710,
The thresholds for both the DE and /RE pins are as follows:
– Max low threshold: 0.8V
– Min high threshold: 2V
Best Regards,
Shane