Post Go back to editing

LTC4332 Is Slave Select (SSx) independent of SCK

Hi,

I would like to use one of the slave select signals as a general purpose digital output (on the slave side) without a SPI data transfer in the same way that the CTRL pin can be used on the LTC4331 (I2C slave extender) LTC4331 DS page 16, Control.

Is this possible?

The LTC4332 data sheet does not seem to indicate if this is possible or not.

Thanks

Mike

Parents
  • Hi Mike, 

    It certainly wouldn't have the same level of flexibility that the LTC4331 CTRL pin has, but it might be possible to use one of the LTC4332 remote slave selects to toggle a function on/off on the remote side.

    More than one slave select cannot be asserted at the same time. One of the slave selects could be held in a given state for a short period. It might be possible to cobble something together with those restrictions. This isn't a function the LTC4332 was previously evaluated for though. 

    Regards,

    Jason  

Reply
  • Hi Mike, 

    It certainly wouldn't have the same level of flexibility that the LTC4331 CTRL pin has, but it might be possible to use one of the LTC4332 remote slave selects to toggle a function on/off on the remote side.

    More than one slave select cannot be asserted at the same time. One of the slave selects could be held in a given state for a short period. It might be possible to cobble something together with those restrictions. This isn't a function the LTC4332 was previously evaluated for though. 

    Regards,

    Jason  

Children