Post Go back to editing

ADUM4154 with 2.5V Vdd

Hi,

From the ADUM4154 datasheet it looks like Vdd can range from -0.5V to 7V. I figure this is a general range, can this device work with Vdd=2.5V and 2.5V SPI signals? Want to check because all examples are with either 5V or 3.3V.

Thanks! 



Changed ranges
[edited by: cdubs1495 at 11:19 PM (GMT -5) on 23 Nov 2020]