Hi,
We are evaluating the ADuM5402.
Please let me ask you a question because it behaved outside the specifications during the experiment.
1. The current consumption of ADuM5402 is recognized as ~ 100mA as shown below.
However, in the experiment, a current of about 250mA (peak) was flowing for about 3.2ms from the time the power was turned on.
Is this normal operation?
2. The current consumption of ADuM5402 tended to increase as the input voltage dropped.
If the input voltage is low (especially at startup / power on), will the current flow more than specified?
In that case, I would like a document that shows the characteristics of the power supply voltage (input) -current consumption of the ADuM5402.
Thank you for your consideration.
Best Regards,
Naohisa