I have a question regarding the input common-mode range of the ADM4168E. The datasheet says the input can swing +/-7V. However the IC is powered by a single 5V supply. Looking at the Rin spec, the condition specifies one input is at 0V, the other can swing +/-7V. So my question is, can the IC really operate with one of the Rx inputs at +/-7V? If so, is there some kind of a resistive divider and/or clamp that allows this to occur? Thanks in advance.