LTM2883
Production
The LTM2883 is a complete galvanic 6-channel digital μModule® (micromodule) isolator. No external components are required. A single 3.3V or 5V supply...
Datasheet
LTM2883 on Analog.com
I am trying to use the LTM2883 for a bidirectional digital interface. One side uses 0 to 3.3V logic and the other side uses 0V to -7V logic. I am new at this, can anyone explain or help me on how to wire this up. The direction is configurable but maintains direction for a long length of time. 2 outputs and 1 input. or 2 inputs and 1 output. It seems like I can use the I2C type hookup.