Post Go back to editing

LTM2883

Thread Summary

The user is attempting to use the LTM2883 for a bidirectional digital interface between 0 to 3.3V logic and 0V to -7V logic. The LTM2883's I/O pins cannot directly interface with 7V logic, violating the Absolute Maximum Rating. For additional bidirectional channels, the ADuM1250 or ADuM2250 are suggested. The user has an evaluation board set up to convert 3.3V to 0V and 0V to -12.5V, which can be adjusted to -7V with a resistor.
AI Generated Content

I am trying to use the LTM2883 for a bidirectional digital interface.  One side uses 0 to 3.3V logic and the other side uses 0V to -7V logic.   I am new at this, can anyone explain or help me on how to wire this up.  The direction is configurable but maintains direction for a long length of time.  2 outputs and 1 input.  or 2 inputs and 1 output.  It seems like I can use the I2C type hookup. 

  • Hi Keith, 

    The LTM2883 is protocol agnostic, meaning it doesn't necessarily need to be used for I2C. But it is only the SDA channel that is bidirectional. The SCL channel only transmits forward. It could be repurposed to support other open collector data though.

    But the LTM2883 can't support a 7V logic directly. That would violate Absolute Maximum Rating. Can you describe the 0V to -7V logic or device that is being isolated?

    Regards,

    Jason  

  • thank you jason,

    The other device is very old and uses 0v as a 1 and -7V as a 0.  It is not happy with less then -6.75V.

    In transmit mode the standard 3.3V logic transmits data and clock at a very slow rate KHz.  The 3.3V side receives an acknolwedge signal in return.

    In receive mode the standard 3.3V logic receives data and clock.  The 3.3V sends the acknowledgement.

    The LTM2883 handles up to +12.5V and -12.5V.  I have an evaluation board and set it up to convert 3.3V to 0V and 0V to -12.5V.  The -12.5 can be changed to -7V with a single resistor.   I have a transmit circuit working to send 0V when the standard logic is 3.3V and -12.5V when the standard logic is 0V.  I was hoping that I could make it work in both directions for all 3 lines.

  • Hi Keith,

    If you need additional bidirectional channels, you can consider the ADuM1250 or ADuM2250.

    Let me clarify the abs max though. The integrated isolated dc/dc converter of the LTM2883 can indeed provide a +/-12.5V supply. But the digital I/O cannot interface with 7V logic directly. That will violate the abs max for the I/O pins.

    Regards,

    Jason