Hi,
I'm a DAFE in Japan. Our customer is interested in ADM2867E due to Low Radiated Emissions. Then he wants to know the data of Radiated Emissions higher than 1GHz. Could you please give us it?
Regards,
Hiroyuki
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADM2867E
Recommended for New Designs
The ADM2861E, ADM2863E, ADM2865E, and ADM2867E are 5.7 kV rms signal and power isolated RS-485 transceivers. These devices are designed for balanced transmission...
Datasheet
ADM2867E on Analog.com
Hi,
I'm a DAFE in Japan. Our customer is interested in ADM2867E due to Low Radiated Emissions. Then he wants to know the data of Radiated Emissions higher than 1GHz. Could you please give us it?
Regards,
Hiroyuki
Hi Hiroyuki,
The data was gathered between 1GHz and 4GHz in anechoic chamber 3m from a horizontal antenna, which is the worst case orientation.
With peak detector the maximum emission from the evaluation board is 57dBuV/m @ 3.7GHz, 17dBuV/m margin to the EN55032 / CISPR Class B limit of 74dBuV/m.
With average detector the maximum emission is 51dBuV/m @ 3.7GHz, 3dBuV/m from the Class B limit of 54dBuV/m.
I am having difficulty sharing images on EZ at the moment, I will follow up with an image of the scan once the sharing issues are resolved.
Regards,
Neil
Hello Neil,
Thank you very much for your support. I wait for your update.
Regards,
Hiroyuki
Hi Hiroyuki,
Please see attached peak scan:
Regards,
Neil
Hi, Thomas from Austria- we have a issue with the radiation at 3.77 and 4.02 GHz, violating RX limits of EN 302 571. Until now we could not identfy if it is emitted directly from the chip or via the PCB. We used the reference design from the Datasheet.
the source is clearly the ADM2867E.
Do you have any hints how to improve this behaviour?
Hi Thomas,
Could you share more details on the emission levels you are seeing with the device? I am surprised to see the 4.02GHz frequency appear from the ADM2867E.
If possible I would recommend reducing the size of the GND2 plane -> This will reduce the antenna area and form a less efficient dipole antenna. If this is not possible and you need a large secondary side ground plane, inductive/ferrite filter can be used to separate an small GND2 plane of the ADM2867E from the rest of the secondary side ground plane.
Regards,
Neil
Hi Neil, thanks for the feedback.
The 4.205 GHz is gone, when Vcc is disconnected. The 3.77 needs Vio and the UART to be down.
the 3.77GHz look like this (Frequency depends slightly on temperature:
I will send the 4.205 when I get it.
Regards,
Thomas
Regarding GND2- we do not have a plane for GND2, it looks like this:
We will interrupt it with an inductor close to the chip and see if it helps.
Regards,
Thomas
Good Morning,
Current finding: any modification on the GND2 structure has no effect on the emission.
Regards,
Thomas
We still do not have any improvement on this topic.
do the slower Versions (ADM2863) have different characteristics in this regard?
One additional comment, the spurious we measure is about the same as shown above in your measurement. Unfortunately we have to test against the Radio emitting standard in RX mode, which is lower.