Hello,
What is the ESD protection levels for ADM232AARNZ-REEL7 part? Does it meet standard +/-15kV ESD protection on Receiver pins?
Regards
Murali
ADM232A
Production
The ADM222, ADM232A, ADM242 are a family of high-speed
RS-232 line drivers/receivers offering transmission rates up to
200 kB/s. Operating from a single...
Datasheet
ADM232A on Analog.com
Hello,
What is the ESD protection levels for ADM232AARNZ-REEL7 part? Does it meet standard +/-15kV ESD protection on Receiver pins?
Regards
Murali
Thank you for your query,
The ADM232A has 1500V protection to the Human Body Model (HBM) standard on all pins.
The ADM202E is a suitable alternative with 15kV ESD protection on the RS-232 pins, to the system level IEC61000-4-2 standard.
https://www.analog.com/en/products/adm202e.html
Regards,
Neil
Hello Neil,
Thanks for your reply.
Does that mean ADM232A needs additional external protection for meeting IEC61000-4-2 standard?
Regards
Murali
Hi Murali,
That is correct, the ADM232A would need external protection, whereas the ADM202E does not need any external protection to meet Level 4 IEC-61000-4-2 protection.
For adding IEC61000-4-2 protection to the ADM232A, something like the SM-15 series of TVS protection components would be suitable, which are available from multiple vendors .
Regards,
Neil