Good afternoon,
I am an electronics engineer working for the CEA in Grenoble (France) and I am actually working on the electronics of a product made for medical applications that was designed few years ago.
We need to pass a special standard for Medical Devices called IEC 60601, that's why our product needs to have good EMC performances.
After testing our product in a EMC laboratory, we observed a heavy peak around 350 MHz that makes us out of the EMC template we need to respect for the standard.
After some investigations, we found out that this high frequency peak was possibly due to digital isolators implemented in the main PCB of our product.
Those isolators are Analog Devices products parts of the "isoPower" devices family.
Here are some of the isolators that were implemented in the PCB of our product: ADuM4190; ADuM4160; ADuM2250; ADuM6404
We recently discovered the AN-0971 Application Note which gives some recommendations regarding radiated emissions when using those products.
This note mentions a 360 MHz peak that is appearing in some worst-case scenario. This peak seems very similar to the peak we observed during the EMC test.
I would like to know if some users have already had trouble with this family of products regarding EMC.
Do you have any recommandations for reducing this high peak without changing completely our design or totally rerouting our board (for example, adding capacitors or inductances at a certain location or adding a kind of metallic shielding over the components) ?
Feel free to ask me if you have any questions of if you need more information and details about our product.
Thank you for your help.
Sincerely,
Antoine.