Post Go back to editing

(ADuM4138/ADuM4137)Differences between the ADuM4137 and ADuM4138

Thread Summary

The user asked about the differences between the ADuM4137 and ADuM4138, particularly regarding fault detection. The ADuM4137 lacks a flyback controller, has multiple fault reporting pins, no PGOOD pin, and removed DESAT protection in favor of an ASC pin. SPI communication in the ADuM4137 requires UVLO_nFault to be driven low. The user also confirmed that using the ADuM4138 on the high side and ADuM4137 on the low side in a daisy chain configuration is possible.
AI Generated Content

Hi!

I would like to see the differences between the ADuM4137 and ADuM4138, but I am still reading the datasheet.

Are there any major feature differences besides having a flyback controller?
For example, the fault detection function is different.
If there are other major differences, please let me know.

Best regards

Kawa