Post Go back to editing

LTM2892 3-wire SPI use

Thread Summary

The user inquired about using the LTM2892 for 3-wire SPI communication, specifically with the AD9634 which uses SCLK, SDIO, and CSB. The support engineer confirmed that the LTM2892 cannot automatically manage bidirectional data on the SDIO pin, leading to potential contention. A suggested workaround involves reducing the drive strength of the LTM2892's output channels to allow the SPI master and slave to dominate when transmitting.
AI Generated Content

Hello

Can the LTM2892 be used for 3-wire SPI?

Is there a circuit example for that?

Thank You

Parents Reply Children
No Data