Hello,
I am trying to use ADuM5028 to supply gate driver with isolated 5V, but I have read in the datasheet in page 11 that "It is recommended that the ADuM5020-3BRWZ and the
.
ADuM5028-3BRIZ are only used for 3.3 V input to 3.3 V operation, therefore connect VSEL
to GNDISO". And in page 15 that "Note that the ADuM5020-3BRWZ and the ADuM5028-3BRIZ can only be used for 3.3 V input to 3.3 V output applications"
Can ADuM5028 operate in 5 V input to %V operation to supply LM5114 gate driver to drive GaN switch EPC2034 appropriately?
Your help is highly appreciated,