ADN4655 unused inputs and outputs

Hello,

I am using ADN4655 in an application to isolate LVDS and I have one input and one output on another IC that are not used. I didn't see any guidelines for the LVDS isolators on what to do with the unused pins. I am assuming the best thing to do for the output is terminate it with 100 ohms, but I'm not sure what the best approach at the input is.

Thanks,

Chris

Parents Reply Children
  • +1
    •  Analog Employees 
    on Jan 24, 2020 4:24 PM in reply to cbradley

    Termination at the input with 100 ohms will be sufficient for ADN4655 and ADN4656. ADN4654 doesn't have the terminated failsafe built-in, so external biasing would be required (pull-up on D+, pull-down on D- to ensure >100 mV for logic 1).

    ADN4655 will output a stable logic 1 when the input is just terminated by 100 Ohm, no other connections/biasing required.