Hi,
I can't find differences between ADM2795EARWZ and ADM2795EBRWZ. Could I ask to explain them?
Regards,
Ivan
ADM2795E
Production
The ADM2795E is a 5 kV rms signal isolated RS-485 transceiver that features up to ±42 V of ac/dc peak bus overvoltage fault protection on the RS-485 bus...
Datasheet
ADM2795E on Analog.com
Hi,
I can't find differences between ADM2795EARWZ and ADM2795EBRWZ. Could I ask to explain them?
Regards,
Ivan
Hi Ivan,
The ADM2795EARWZ is rated to a maximum ambient temperature of 85C.
The ADM2795EBRWZ is rated to a maximum ambient temperature of 125C.
Other than this the devices are identical
Regards,
Neil
Hi Neil,
Thank you for the explanation.
Regards,
Ivan