Hello, I am designing an inverter using ADUM6132 gate driver. I have two questions.
Data sheet does not say much about dead-time. Is it possible to create dead-time inside adum6132 or should I leave dead-time for signals going to the adum6132 as input?
My second question is that there seems to be two power supply needed for adum6132. 5V for one and 15V for another, nominally. Is it possible to set configuration with voltage divider? I am saying that I will supply +15V externally and use voltage divider to create +5V out of +15V and then use these two as input to adum6132. Would it work?
Thank you in advance,
Alper
Hello Alper,
The ADuM6132 has two independent inputs, VIA and VIB. Any deadtime needs to be introduced from the controller side. If VIA and VIB are both held high at the same time, both outputs will be…