The attached Japanese errata mention the capacitor withstand voltage value of C3 of ADM1385 is 6.3V wrong and 10V is correct.
Is the capacitor withstand voltage of C3 in ADM3202 datasheet correct at 10V ?
ADM3202
Production
The ADM3202 / ADM3222 / ADM1385 are high speed, 2-channel RS232/V.28 interface devices which operate from a single +3.3 V power supply. Low power consumption...
Datasheet
ADM3202 on Analog.com
ADM1385
Production
The ADM3202 / ADM3222 / ADM1385 are high speed, 2-channel RS232/V.28 interface devices which operate from a single +3.3 V power supply. Low power consumption...
Datasheet
ADM1385 on Analog.com
The attached Japanese errata mention the capacitor withstand voltage value of C3 of ADM1385 is 6.3V wrong and 10V is correct.
Is the capacitor withstand voltage of C3 in ADM3202 datasheet correct at 10V ?
Hi,
In datasheet, the C3 is placed between VCC and V+ of ADM3202, so the capacitor with 6.3V rating is OK to use.
Regards,
Neil
Hello Neil
Thank for your reply. I am FAE of distributor.
I want to confirm the attached Japanese errata.
First page of it mentions the capacitor withstand voltage value of C3 of ADM1385 is 6.3V wrong and 10V is correct.
Is this errata wrong?
Best regards
NobuyukiPDF
Hi Nobuyuki,
The errata is right about the voltage rating(10V) of C3 for ADM1385, it is consistent with what shows on the datasheet.
Regards,
Neil
Hello Neil
Thank you for your quick reply.
Is it right the flowing my understanding?
The voltage rating of C3 for both ADM1385 and ADM3202 needs 10V between V+ and GND.
The voltage rating of C3 for both ADM1385 and ADM3202 needs 6.3V between V+ and VCC.
Regard
Nobuyuki
Hi Nobuyuki,
Yes, you are right.
Regards,
Neil
Hi Neil
I appreciate your support.
regards
Nobuyuki.
Hi Neil
I appreciate your support.
regards
Nobuyuki.