Hello,
I am currently using the ADuM6028-5BRIZ and there seems to be an issue with the output voltage.I tested several of my prototype PCBs, but it just doesn't work.
I connected the chip just like the datasheet says:Pin PDIS connected to GND.Vdd is 5V.VSEL is connected to the V_iso pin.
Anyone else got this problem?
Does the chip have some kind of failstate, or overcurrent state, in which the output voltage is shut off?
Thanks!
Best regards
Max
Max: I'm not sure what the problem is, the ADuM6028 should start up and give you a 5V VISO voltage when VSEL is connected to the V_iso pin, using the circuit from the datasheet. Can you send me your…
Max: I'm not sure what the problem is, the ADuM6028 should start up and give you a 5V VISO voltage when VSEL is connected to the V_iso pin, using the circuit from the datasheet. Can you send me your schematic and layout of the ADum6028 circuit? A scope waveform of the VDDP and VISO pins in startup would help too.
Regards, Brian
Max: I am waiting for your response so I can help assist.