Post Go back to editing

Please tell us about the specs of ADuM4122 → High-side to low-side differential voltage

Thread Summary

The user inquires about the 'High-side to low-side differential voltage' for the ADuM4122 dual gate driver. The final answer clarifies that the ADuM4122 has only one isolated output region, so this parameter is not applicable. The ADuM4122's working voltage (Viorm) is 849 V peak, as specified by VDE V 0884-10. For a half-bridge setup, two ADuM4122 ICs are required.
AI Generated Content

Hi, I would like to use ADuM4122.

So, I have a question. Please help me.

Question:

I am considering dual gate drivers.

An important parameter for selection is “High-side to low-side differential voltage”.

In the same category products ADuM7234 and ADuM4223,
It is described in the data sheet.

The above specifications were not written in the data sheet in ADuM4122, so please tell me.

Best Regards,

Naohisa

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.