Hi ,
I would like to know the Max and min Switching frequency of ADUM5010 when using between -40 to 85 degree .
Could you also let me know if you have information with regards to Start up time for 5V input to 5V output or 5V input to 3.3V output .
Thanking you
With best regards and wishes
Kabekami-san:
I received the answer to your question from the designer about the switching frequency of the ADuM5010:
The tank oscillation frequency range is about 150MHz~220MHz under all process, with…
Kabekami:
I have asked your question on the switching frequency to the designer and I am waiting for an answer back.
As far as startup time, it is approximately 3msec for the ADuM5010 output voltage t…
As far as startup time, it is approximately 3msec for the ADuM5010 output voltage to rise up after the input voltage is above the under voltage lockout (UVLO) voltage..
Regards, Brian
The tank oscillation frequency range is about 150MHz~220MHz under all process, with datasheet specified voltage and temperature (PVT).
Brain:
Thank you for the information .
Hi Brian ,
I am sorry i missed to check the data sheet .
The Typical switching frequency is 125MHz in data sheet but your answer was 150MHz~220MHz.